How many operations is an undervoltage trip rated for in a PowerPact H, J, or L frame breaker?
Product Line:
Molded Case Circuit Breaker
Resolution:
The UVR is rated for half the breaker's operations. Below are the amount of operations each breaker frame size is rated for.
| Frame Size (A) | Full Load Operations | No Load Operations |
| 0-100 | 6,000 | 4,000 |
| 101-225 | 4,000 | 4,000 |
| 226-600 | 1,000 | 5,000 |
Released for: Schneider Electric Canada