Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the HOM breakers motor rated?

Issue: Clarification-Product features

Product Line: HOM breakers

Resolution: We have no known issue of using these breakers with motor loads. If the breaker matches the rating of the overload protection then they should be able to use these breakers. Another thing for the motor is that it produces inrush current the trip curve is on our website for the customer to review if it allows the inrush of their motor.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings