How can we help you today?

Where to find dimensions for 9001KYSS & 9001KYAF enclosures?

Issue:

What is the dimension for 9001KYSS1?

Product Line:

Push Buttons and Operator Interface

Environment:

30mm Product line

Resolution:

Height Front - 4.45 inches / Back with mounting holes 4.61 inches

Width - 4.17 inches

Depth - 3.62 inches

KYSS / KYAF enclosure

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: