How can we help you today?

What is the replacement motor for Erie AG Type Actuators?

Issue:

Need to replace the motor in an Erie AG actuator

Product Line:

Erie PopTop Actuators

Resolution:

The part numbers will depend on the voltage rating of the Erie Type G Actuator.

For 24V, part number of the replacement motor is 30-158-A

For 110V, part number of the replacement motor is 30-158-B

For 208V, part number of the replacement motor is 30-158-D

For 277V, part number of the replacement motor is 30-158-T

For 230V, part number of the replacement motor is 30-158-U

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings