Is tin plated CU bus is the same as hard-drawn copper?
Issue:
The definition of tin tin-plated CU bus and hard-drawn copper
Product Line:
LV Panelboards
Environment:
NQ, NF & ILine Panelboards
Resolution:
Tin Plated simply means we cover the bus Copper bars with Tin.
Hard-drawn is a manufacturing practice that has nothing to do with the type of plating we cover the bars with.
See the attached file.
Released for: Schneider Electric Canada