How can we help you today?

Tesys Giga LC1G Remote Wear Diagnostic modules

Issue:

Does LC1G185EHEN have Remote Wear Diagnostic functionality?

Product Line:

Contactors and Starters

Environment:

Tesys Giga LC1G product lines

Resolution:

The LC1G185EHEN is the standard version, it does not have the embedded wear diagnostic functionality. Need to use the advanced version - LC1G185EHEA + Remote Wear Diagnostic (RWD) Module LA9GRD01 (NC contact) or LA9GRD10 (NO contact)

LC1G Advanced version

Remote Wear Diagnostics

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: