Is there a side bonding jumper on the secondary side of an EXN transformer?
Product Line:
EE/EX/EXN Transformers
Environment:
Low Voltage Transformers
Cause:
Bonding jumper for EXN45T3H (NEC 250.102)
Resolution:
The EXN Transformers are shipped with no lugs or terminal hardware whatsoever. Lug installation as well as grounding and bonding are to be performed if needed by the installer or contractor, using lugs and hardware or jumpers provided by them.
Released for: Schneider Electric Canada