Are I-Line cover/trim like the HCW86TS made of stainless steel?
Issue:
Is HCW86TS I-Line cover/trim made of stainless steel?
Product Line:
Panelboards
Environment:
I-Line Panelboards
Cause:
Product Characteristics
Resolution:
All trim fronts/doors are made with black steel and painted with a 9-stage E coat paint system. All of our enclosures and trims are made of sheet metal.
Stainless steel panels are available as factory-assembled options. It should be configured in SE Advantage.
Released for: Schneider Electric Canada