How to program a local/rem (HOA) switching function on the ATS480 softstater?
Under Complete settings, command channel menu 3.8, find command switching, command channel 1 and 2 settings.
Command switching is used to toggle between channel 1 and channel 2. You can set this to a digital input that will act as your command switching.
When that input is toggled, the unit will look at second channel away from first channel for controls.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Canada