Can a QO2200, QO2150, and a QO2175 breaker be added to a NQSE142400S?
Issue:
Can a QO2200, QO2150, and a QO22175 breaker be used in an NQSE panelboard?
Product Line:
NQ and NQSE Panelboards
Resolution:
Yes, the QO2200, QO2150, and the QO2170 breakers can be added in any 400A NQSE interiors.
See the attached file for the restrictions.