How can we help you today?

What does the "-770" mean in VB-7253-770-4-11?

Issue:

Is the "-770" in VB-7253-770-4-11 an actuator code?

Product Line:

Valves and Actuators

Resolution:

The -770 means the valve is sold to Belimo and is not an actuator code.

All VB-7000 series valve with the -770 in the part number are valve bodies only sold to Belimo with the Belimo part number on the valve tag.  This is like the  VB-7XXX-770-4-XX valve part number style

Schneider Electric Canada
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
  • Product Selectors