How can we help you today?

What are the Options to Mount a GV4 Motor Circuit Protector?

Issue:

To find out what are the mounting options of a GV4 Motor Circuit Protector

Product Line:

GV4 Motor Circuit Protector

Environment:

IEC Contactors and Starters

Resolution:

A GV4 device has an option to be mounted for both din rail or panel mounted.

For Din Rail Mounting, it requires 35mm din rail or a 75mm din rail.

Din Rail Mounting

For Panel Mounting, it uses M4 screws.

Panel Mounting

For complete instruction sheet, see link below:

EAV91200-03

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: