How can we help you today?

Can a 1200A rated solid neutral assembly be used in an 800A I-line panelboard?

Product Line:

I-Line 1200A solid neutral assembly


Environment:

I-Line Panelboard


Cause:

Need to confirm if HCP12SNALCU neutral assembly be used in an 800A HCP panelboard


Resolution:

It won't fit into the designed location using the designed mounting holes, but it could be field installed in some open area inside the box.


Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: