How can we help you today?

Will it void the warranty if the NQ panelboard is painted over?

Issue:

Could the NQ panelboard be painted over?


Product Line:

NQ Panelboard


Resolution:

We offer painted for the factory assembled panel so painting them in the field is not an issue. The labels have to be taped off as they can not be replaced in the field. Also, there are no warranty issues but make sure none of the labeling gets painted over and no overspray gets on the breakers or other components behind the interior deadfront.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings