What are the exterior finish options or RAL numbers available for PZC E-House Enclosures for switchgear?
Issue:
Need to see if there is a catalog for the available RAL colors.
Product Line:
E-House Enclosures.
Environment:
Switchgear
Resolution: We have the capability to paint the E-House in any color required by the client, provided it matches a Sherwin Williams or Dupont paint number. To facilitate this, we kindly request the specific paint numbers or a paint sample (paint chip) to be forwarded to the engineering team during the construction phase. It's important to note that there may be an additional charge for custom colors, with the cost varying based on the color chosen. The available color options are quite flexible, and while white or gray are standard and do not incur an extra charge, any non-standard colors may involve an additional cost. Therefore, for any specific options, such as those found in a catalog, we recommend consulting with paint manufacturers for available choices. Reach out to your local sales representative or distributor to inquire about any associated cost adders.