Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ZB4/ZB5 TQ Suffix

Issue:

Find out what the TQ Suffix indicate on the ZB4/ZB5 Part Numbers


Product Line:

22mm Harmony Push Buttons and Selector Switches


Environment:

Push Buttons and Operators


Resolution:

TQ Suffix indicates bulk packaging. The part number without TQ is just the same as the one with TQ. The main difference is the part with TQ comes in a set of 100 packaged in one big box unlike the one without TQ suffix which comes in individual packaging.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings