How can we help you today?

GS2MU3N Fused Disconnect Mounting Orientation

Issue:

GS1 and GS2 Mounting Orientation

Product Line:

Operating Mechanism and Disconnect Switches

Environment:

GS Fusible IEC Style Disconnect Switches

Cause:

No reference document for GS1 and GS2 if can be mount on Horizontal Position.

Resolution:

The disconnector switch GS1-GS2 can be mounted in several positions, can be rotated by step of 90° according to the picture below.

Please see attached image.

Schneider Electric Canada

Attachment(s)
GS1-GS2 Orientation.png [100.06 KB]