How can we help you today?

How to Change configuration Settings on the Climasys CC - Electronic Hygrotherm

Product Line:
Thermal Management Systems and ClimaSys

Environment:
ClimaSys CC Temperature Controller

Cause:
Profile configuration and temperature setting may be different than desired for the application, it can be modified on the hygrotherm

Resolution:

Hygrotherm work in 3 different profiles, (M1 /M2 /M3)  M1 comes by default programmed:

Operating Modes

  • M1 Ventilation/Humidity and temperature control
  • M2 Dew Point Control with alarm
  • M3 Differencel Cools/Heats with the exterior temperature /Humidity and Temperature Control

To modify the current profile parameters the current Operating Mode (M1/M2/M3) will cycle the different setting you can modify, when the desired value to change shows on the screen you will need to press Up or Down Button to adjust the Temperature, Dew Point, Humidity and % values according to parameter and confirm with the center PAGE button to confirm modifications.

Depending on the operating mode selected it would have the respective temperature ranges this goes linked to the Celsius and Fahrenheit version on the temperature controllers, to verify that our changes were made yo can perform a power reset to establish the controller.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings