Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
TeSys T How to enter configuration mode via SoMove and get to Ready Status on the LTMR

Product Line:
Industrial Automation Control

Environment:
Motor Management Systems TeSys T

Cause:
How to Enter/Exit configuration mode on the TeSys T via SoMove and save modified parameters on the LTMR controller

Resolution:

Configuration Mode it´s a state on which the controller (LTMR) will allow us to freely modify and change parameters and configuration setting on the current connected controller, for this it is mandatory that a correct communication has been established, and that out program data is currently synchronized.

data synchronized

Once our data is synchronized and a stable communication path has been made with the LTMR and SoMove we will have a READY state showed on the foot of the software.

To enter configuration mode, we will click on our top tab that called DEVICE -> COMMAND -> ENTER CONFIGURATION

Entering configuration mode SoMove

We can confirm that we entered  configuration mode successfully if our READY state has been changed to In Config

In Config SoMove

Entering this state will unlock all parameter setting to be changes and modified as needed, once our changes are made and we´re ready to load them into the controller, we will exit configuration mode on the same path DEVICE -> COMMAND -> Exit Configuration Mode -> Yes

Exit Configuration Mode

After confirming exiting configuration mode our device state will go back to READY state after a brief moment and changes will be done to the program, we suggest doing a last Load to Device in order to match any modification SoMove <-> Controller.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings