Can Harmony 3 phase control relays be used to monitor Variable Speed Drives?
Issue:
Can Harmony 3 phase control relays be used upstream or downstream a Variable Speed Drive (VSD)
Product Line:
Harmony Control Relays
Environment:
RM17, RM22, RM35, 3 phase control relays
Cause:
It’s not recommended to operate the RM17/RM22/RM35 products with VFD or VSD systems as the noise interference from the VFD/VSD can cause damage to the contol relay.
Resolution:
Do not connect 3 phase control relay to monitor output of Variable Speed Drive (VSD).
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.