How can we help you today?

Zelio Programming: How to properly Stop a program that´s currently running and how to make the program Run Again using the relay´s display.

Product Line:
Zelio Smart Relays

Environment:
Rail Mounted Programmable smart Relays

Cause:
How can we Start or Stop a program that currently installed into a zelio relay with display screen.

Resolution:

To properly STOP a program that´s currently running we will need to navigate the display using the (Right/Left/Up/Down/Menu/Ok) Buttons, according to the standard screen of a running device you will see the following:

It is mandatory that your commercial reference smart relay has a front panel display screen and buttons to proceed with this.

Default layout screen for zelio relays

Program in stop mode zelio

In STOP mode: The program is stopped and the outputs disabled

To run the program we will navigate with out DOWN arrow button and once we are selecting RUN/STOP we will click our green button Menu/OK and we´ll be taken to the following screen:

Run Program Zelio

In STOP mode, when accessing the RUN/STOP menu, the interface proposes the following three choices for starting the program:

WITH NONVOLAT INI: All values (counters, timers, etc.) are reset to their initial values before the program starts (default selection),

NO NONVOLAT INI: Values for which the Latching option has been activated are kept,

NO: The program does not start.

In RUN mode, when accessing the RUN/STOP menu, you need to confirm the request to stop the program:

YES: The program stops (selected by default),

NO: The program does not stop.

Stop program state

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings