How can we help you today?

Zelio Smart Relay: Program Construction Error

Issue:

ZelioSoft 2 shows the "Prorgram construction error" when transferring the program from the relay to the PC.

Product Line:

Relays and Timers

Environment:

Zelio SR2 and SR3 Smart Relays

Resolution:

There are certain cases where the program cannot be retrieved and Zeliosoft 2 shows the following "Program construction" error:

Program construction error message

ZelioSoft should rebuild the application with following limitations:

  • Construction using the file specified by the user: enter the file path of the application to be retrieved.
  • Automatic construction of the program: In this case, the Programming Software regenerates the application from the data retrieved on the smart relay.
NOTE: The program loaded into the smart relay does not contain information concerning page setup (drawing, comment, relative position of the function blocks and links); a default page setup is thus produced.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings