Documentation for EM3570 series Energy Meter
Issue
Where to find documentation for the EM3570 series Energy Meter
Product Line
METSEEM3570
METSEEM3570A
METSEEM3570X
METSEEM3570AX
METSEEM3570PS
METSEEM3570ENC
Environment
EM3570 Energy Meter Series Documentation
Cause
Where to download documents regarding the EM3570 Energy Meter Series
Resolution
The following EM3570 Series documents are available:
METSECTRx Series Rogowski Current Transducers Instruction Sheet
PowerLogic™ UL 2808 LV Current Transformers (LVCT)
Modbus Register List (Modbus Point Map) (see attachment)
Customer BACnet ID (see attachment)
EM3570 UL Certificate of Compliance (see attachment)