What is the catalog number for the lugs used on the NQN6CU kit?
Product Line:
NQ Panelboard
Environment:
Low Voltage Panelboard
Cause:
Replacement neutral lug for NQN6CU kit.
Resolution:
The NQN6CU uses Cat# NQNFRPLALMN46 lug. The lug wire range for that neutral assembly is (1) #1/0 to 750 kcmil. Al or Cu wire. It can also accommodate two wires per lug but it limits the wires size to 300kcmil max only.