What does the JK or JA suffix means on M, P, or R frame breakers?
Issue:
Kirk interlock for M frame breaker
Product Line:
Molded Case Circuit Breakers
Answer:
JK or JA suffix are provisions for installation of Kirk Key Interlocks on the breakers. JA is for vertical mounting and JK is for horizontal mounting