What is the wire range of mechanical lug kit AL150HD?
Issue: Identifying the wire range of the mechanical lug kit AL150HD
Product Line: PowerPacT H-Frame Molded Case Circuit Breaker
Resolution:
The mechanical lug kit AL150HD has a wire range of (1) 14–3/0 AWG aluminum or copper per phase. This is only compatible with 15–150 A, H-frame circuit breakers.