How can we help you today?

What Are The Replacement Control Modules for Tesys Giga Contactors?

Issue:
Part numnber for changing the control voltage, convertion from standard to advanced (and vice versa), or replacement in case of a malfunction of control modules for Tesys Giga.

Product Line:
Contactors & Starters

Environment:
Tesys Giga

Resolution:

The control module contains the components required to control the contactor
poles:
• A fixed magnetic circuit
• a coil winding
• an electronic board

There are two types of the control modules:
• Advanced control module
• Standard control module

The control module can be replaced by a spare control module:
• to change the control voltage of the contactor
• to convert a standard contactor in an advanced contactor, and vice versa
• to replace a control module after detection of an internal malfunction

Below are the references.

Advanced Control Modules
ContactorControl Voltage3-Pole control module4-Pole control module
LC1G115–22524–48 Vac/VdcLX1G3QBNEALX1G4QBEEA
48–130 Vac/VdcLX1G3QEHEALX1G4QEHEA
200–500 Vac/VdcLX1G3QLSEALX1G4QLSEA
LC1G265–33024–48 Vac/VdcLX1G3RBNEALX1G4RBNEA
48–130 Vac/VdcLX1G3REHEALX1G4REHEA
200–500 Vac/VdcLX1G3RLSEALX1G4RLSEA
LC1G400–50024–48 Vac/VdcLX1G3SBNEALX1G4SBNEA
48–130 Vac/VdcLX1G3SEHEALX1G4SEHEA
200–500 Vac/VdcLX1G3SLSEALX1G4SLSEA
LC1G630–80048–130 Vac/VdcLX1G3TEHEALX1G4TEHEA
200–500 Vac/VdcLX1G3TLSEALX1G4TLSEA
Standard Control Modules
ContactorControl Voltage3-Pole control module4-Pole control module
LC1G115–22548–130 Vac/VdcLX1G3QEHENLX1G4QEHEN
100–250 Vac/VdcLX1G3QKUENLX1G4QKUEN
LC1G265–33048–130 Vac/VdcLX1G3REHENLX1G4REHEN
100–250 Vac/VdcLX1G3RKUENLX1G4RKUEN
LC1G400–50048–130 Vac/VdcLX1G3SEHENLX1G4SEHEN
100–250 Vac/VdcLX1G3SKUENLX1G4SKUEN
LC1G630–80048–130 Vac/VdcLX1G3TEHENLX1G4TEHEN
100–250 Vac/VdcLX1G3TKUENLX1G4TKUEN