How can we help you today?

Equalize parameter not visible on SCP

The Equalize parameter should be visible in the SCP (System Control Panel) settings where it gives you the option to enable or disable it. If you do not see it, check the battery type under charger settings. If the Battery Type is set to Custom, you need to enable equalize support to allow equalizing under the custom battery settings, and then you can see the equalize parameter.
Note: When the system is set to Custom, as a safety precaution to make sure you are not equalizing the wrong set of batteries, you have to enable an additional parameter to equalize batteries.