How can we help you today?

How to Replace the Obsolete Control Module 3110408250?

Issue:

The control module for NEMA size 6 contactors and starters occasionally require replacement

Product Line:

NEMA Contactors and Starters

Environment:

Type S Full Voltage Contactors and Starters

Resolution:

The reference 3110408250 was the control module for ALL early 8502/8536 Size 6, Series B contactors and starters. The control module is used to develop the two DC voltages used by coil to pick the armature up and to keep it sealed (closed). 31104-082-50 is obsolete.

Use kit part number 3112351450 as a direct replacement. Kit part number 31123-514-50 includes the current control module (3112301750) and installation instruction sheet 30072-010-04B. See attached.

Schneider Electric Canada

Attachment(s)
30072-010-04b Instruction sheet.pdf [1.14 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: