How can we help you today?

Are there Time Delay Auxiliary Contact Blocks for LC1D Contactors with Low Consumption Coils?

Issue:

Not all TeSys™ Deca contactors may use the front mount time delay contact blocks

Product Line:

TeSys™ Deca Contactors

Environment:

Contactors and Starters-IEC

Resolution:

Except for the LC1D09* to LC1D38* models with low consumption coils, all other LC1D* contactors can use a front mount time delay auxiliary contact block. A contactor with low consumption coil has one of the following suffix: AL, JL, ZL, BL, EL, SL, DL, FL, ML, and UL - for example LC1D09BL.

Pneumatic Time Delay Contact Blocks
TypeRange of
Time Delay
Catalog Number
On energization (on delay)0.1 to 3 s LADT0
0.1 to 30 s LADT2
10 to 180 s LADT4
1 to 30 s LADS2
On de-energization
(off-delay)
0.1 to 3 s LADR0
0.1 to 30 s LADR2
10 to 180 s LADR4