How can we help you today?

What Is The Possible Reason a GV4AE11 Does Not Change State?

Issue:

The GV4AE11 may not work as intended

Product Line:

TeSys™ Deca GV Manual Starters and Protectors

Environment:

Contactors and Starters-IEC

Resolution:

The functionality varies depending on the section it is installed.

On the right cavity which where it is currently installed, it functions as "TRIP Indicator".

For instantaneous function, the left cavity should be used. To have the auxiliary contacts change the same time when the motor protection device is turned on, use the left slot instead of the right.

GV Motor Starter

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: