How can we help you today?

What are the Parts Included on XB5R and XB4R Programmable Ready-to-use Packs?

Issue:
XB5R and XB4R Ready-to-use packs occasionally require parts replacement

Product Line:
XB5R Plastic and XB4R Metal Wireless, Batteryless Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:

Please see parts breakdown below.

XB5RFA02
ZBRRA - Programmable receiver
ZBRT1 - Transmitter
ZB5AZ009 - Plastic mounting collar
ZB5RZA0 - Flush push type spring return push button head in plastic (without cap)
ZBA79 - Set of 10 different colored caps

XB5RMA04
ZBRRA - Programmable receiver
ZBRT1 - Transmitter
ZB5AZ009 - Plastic mounting collar
ZB5RZA0 - Flush push type spring return push button head in plastic (without cap)
ZBA79 - Set of 10 different colored caps
ZBRM01 - Handy box

XB4RFA02
ZBRRA - Programmable receiver
ZBRT1 - Transmitter
ZB4AZ009 - Metal mounting collar
ZB4RZA0 - Flush push type spring return push button head in metal (without cap)
ZBA79 - Set of 10 different colored caps

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: