How can we help you today?

Do Transformers (EX, EXN, 9070, MPZ, MPU) have UL 94 Rating?

Issue:

Need to know if the 9070 control transformer conforms to the UL 94 rating.

Product Line:

LV Transformers

Environment:

Applies to Transformers by SquareD/Schneider Electric

Cause:

Low voltage Transformer UL ratings

Resolution:

Square D/Schneider Electric has done no flammability testing on 9070 Transformers, as the UL94 test relates largely to the plastic content of a product.

For that reason, there is no such document for 9070s or any other Transformer product. Transformers have relatively little, and are mostly steel and copper wire, so the need has not typically arisen to rate the Transformer products according to that standard.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings