Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the HPDM6000 Head Unit support multiple source voltages for metering?
Issue
I would like to connect multiple source voltages to the HDPM6000 Head Unit.
For example: 480Y/277V system and 208Y/120V system to be metered with one HDPM6000 Head unit.
Product Line
HDPM6000 Series
Environment
HDPM6000 Head Unit
Cause
I want to monitor a 480Y/277V system and 208Y/120V system with one HDPM6000 Head unit.
Resolution
The HDPM6000 Head unit is designed to monitor only one single source voltage.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings