Can BMXDDI1602H be used to replace BMXDDI1602?
Issue:
Do I need to replace BMXDDI1602 with same part number or I can use BMXDDI1602H ?
Product Lines:
Modicon x80 module
Environment:
All serial numbers
Resolution:
Yes, the BMXDDI1602H can be used to replace the BMXDDI1602. The BMXDDI1602H is the ruggedized version of the BMXDDI1602, designed for operation in extended temperatures and harsh chemical environments, making it suitable for more demanding conditions while maintaining compatibility with the standard BMXDDI1602 module.
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.