In EcoStruxure Operator Terminal Expert, why do my String Displays not show the text and symbols from String Variables from Modicon M241/M251/M262 PLCs?
Issue:
On my HMI Display running EcoStruxure Operator Terminal Expert, the String display is showing blank values or incorrect characters when reading from STRING type variables using the Schneider-MachineExpertNetwork driver reading from a Modicon M241, M251 or M262 PLC.
Product Line:
EcoStruxure Operator Terminal Expert
EcoStruxure Machine Expert
Environment:
HMI Configuration Software in Windows
Resolution:
For the HMI to read the STRING and WSTRING type variables via MachineExpertNetwork protocol,
- In EcoStruxure Operator Terminal Expert software, open your HMI project
- Navigate to the Project Explorer
- Expand Target01 > Drivers
- Select "Schneider Electric-MachineExpertNetwork*" node
- In the System Architecture page, click on the row of the Equipment (default name "MachineExpertEquipment1")
- On the far right side of the screen under the Properties box, find "String Encode" near the bottom of the list.
- In the String Encode dropdown, select "CodePage1252"
- Download the changes to your HMI (or Simulate)
ALSO NOTE: The best font to use for String Displays showing String Variables from M2xx PLCs is <LanguageName>_Gothic
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.