Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What cable do I use for Modbus Serial Communication between Harmony HMIST6 / HMISTM6 and BMXP341000/2000/2020?

Issue:

I would like to establish Modbus Serial Communications between a Harmony HMIST6 or HMISTM6 series HMI and a Modicon M340 PLC with the front RJ45 Modbus Serial Port (Part Numbers BMXP341000, BMXP342000, BMXP342020). What cable do I use?

Product Line:

Harmony HMIST6: HMIST6200, HMIST6400, HMIST6500, HMIST6600

Harmony HMISTM6: HMISTM6200, HMISTM6400

Modicon M340: BMXP341000, BMXP342000, BMXP342020

Environment:

Modbus Serial Cabling between HMI and PLC

Resolution:

This table below lists all possible connection types between the HMIST6/HMISTM6 models and the M340 PLC with the associated required Serial Cable:

HMI Part NumberHMI Serial PortSerial Communication StandardCable Part Number
HMIST6200COM1 (RJ45)RS-485XBTZ9980
HMIST6400COM1 (Dsub9)RS-232TCSMCN3M4F3C2
HMIST6400COM2 (RJ45)RS-485XBTZ9980
HMIST6500COM1 (Dsub9)RS-232TCSMCN3M4F3C2
HMIST6500COM2 (RJ45)RS-485XBTZ9980
HMIST6600COM1 (Dsub9)RS-232TCSMCN3M4F3C2
HMIST6600COM2 (RJ45)RS-485XBTZ9980
HMIST6700COM1 (Dsub9)RS-232TCSMCN3M4F3C2
HMIST6700COM2 (RJ45)RS-485XBTZ9980
HMISTM6200COM1 (RJ45)RS-485XBTZ9980
HMISTM6400COM1 (RJ45)RS-485XBTZ9980

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings