How can we help you today?

What is the Difference Between ZBE1015 and ZBE1015SC?

Issue:
ZBE10*5, ZBV**5, ZB4BZ*5, ZB5AZ*5 design change

Product Line:
22 mm Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:

Effective February of 2025, the reference ZBE1015 that used to have spring clamp terminals has been updated to a compact push-in contact block. Spring clamp terminal blocks are still available with with references having "SC" suffix.

Key Benefits of the New Design:
- use modern push-in technology for wiring the product as opposed to requiring the manual press of a spring clamp lever mechanism
- height decrease by ~20%
- allows the contact blocks to be stackable

ZBE10*5, ZBV**5, ZB4BZ*5, ZB5AZ*5  - push in terminals
ZBE1015SC and ZBE1025SC - spring clamp terminals

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings