How can we help you today?

Is It Normal for the LAD703* and LA7D03* Relay to Emit a Buzzing Sound?

Issue:
Buzzing noise from LAD703*and LA7D03* modules

Product Line:
Overload Relay Accessories

Environment:
TeSys™ Deca Overload Relays

Resolution:
Both LAD703* and LA7D03* are references for remote stop/tripping or electrical reset compatible for TeSys™ LRD/LR3D overload relays. It is normal for these modules to produce a fairly loud audible buzz when they operate.