Piano-Hinged Doors and Covers for NEMA 1 NQ and NF Panelboards
Issue:
Clarification on the availability of piano-hinged door and cover options for NEMA 1 NQ and NF panelboards.
Product Line:
NEMA 1 NQ and NF Panelboards
Cause:
Users may require hinged access for ease of maintenance or inspection, and need to know the available configurations.
Resolution:
Yes, there are options available. Both surface-mounted and flush-mounted doors/covers for NEMA 1 NQ and NF panelboards are piano-hinged. To select the appropriate style, choose either Surface-hinged or Flush-hinged in the selector.