How can we help you today?

What is the maximum frame breaker that can be installed on a I-line QED2 section?

Issue:
The maximum frame breaker that can be installed on an I-line QED2 section

Product Line:
QED2 Swithboards

Resolution:

Max 1200A Breaker R Frame/ P Frame

I line QED2

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings