What are the end cap fittings for RWT10S60?
Subject:
End Fittings for RWT10S60 Wall Duct
Language:
English
Issue:
Identifying the correct end fitting for RWT10S60
Product Line:
Schneider Electric Wall Duct Accessories
Resolution:
The catalog number for the End Cap Fitting used with the RWT10S60 wall duct is RWT10EC.
To find this and other related fittings or dimensions:
- Refer to the Wall Duct Catalog Class 5250 available below.
- The RWT10EC End Cap Fitting is shown on page 13 of the catalog.
- Customers can search for “Wall Duct Class 5250 Catalog” or use catalog number 5250CT9201 on se.com to locate the document.