Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a door for a QED switchboard that opens 180 degrees instead of the standard 90 degrees?

Article available in these languages: Spanish

Issue:
Is there a door for a QED switchboard that opens 180 degrees instead of the standard 90 degrees?

Product Line:
QED Switchboards – Schneider Electric

Environment:
Commercial and industrial electrical distribution systems

Cause:
Customer requires wider door access for maintenance or operational convenience.

Resolution:
Schneider Electric does not offer any hinges that allow a QED switchboard door to open 180 degrees. The standard configuration supports a 90-degree door opening only.

Internal Reference No:
CR-6230142