Correct Wiring for External CT with LTMR Devices
Title:
Correct Wiring for External CT with LTMR Devices
Issue:
How should the external current transformer (CT) be wired to the LTMR device?
Product Line:
LTMR (Motor Protection and Control Devices)
Environment:
LTMR device with external CT connection (CT terminals labeled S1/S2)
Resolution:
Your CT must have two terminals (S1 and S2). The wiring should be as follows:
- The wire must leave S1, pass through the internal CT of the LTMR, and then land on the second terminal S2.
This ensures proper current measurement and device functionality.