Flammability Rating for ZBE1029 Contact Block
Title:
Flammability Rating for ZBE1029 Contact Block
Issue:
What is the flammability rating for the ZBE1029 contact block?
Product Line:
ZBE Contact Blocks
Environment:
Standard industrial control applications using ZBE1029 contact blocks
Resolution:
The ZBE1029 contact block is made of PA6 GF20 material and has a flammability rating of V-2. It is also halogen-free.