How can we help you today?

How to Mute a Back UPS ™ ES M unit?

Question:

How to Mute a Back UPS ™ ES M unit?

Product Line:

BW650U1, BN450MNW, BVN900M1, BVN650M1, BE850G2, BE600M1, BE425M, BE850G2, BN450M, or any of the units that has the same form factor as shown in the image below.

Image of the Back UPS form factor being discussed in this FAQ Article

Resolution:

There are three main ways to mute alarms on Back‑UPS products, as described in this article. You can:

  1. Use Quick Mute,
  2. Manually customize the On‑Battery alarm settings on the UPS, or
  3. Disable the alarm through PowerChute™ Serial Shutdown (PCSS).

Option 1 : Quick Mute

The Back-UPS ™is able to temporarily mute user correctable alarms such as On Battery. During such alarms, a short press (less than 2 seconds) of the POWER button will temporarily mute the alarm until the condition has been reset. A short double beep will confirm that Quick Mute has been activated. Pressing the POWER button for more than 2 seconds will turn off the UPS. Other critical events such as Battery replacement and Charger notification can not be temporarily muted. The unit in these cases must be turned off.


Option 2 : Customize On Battery Alarm Settings

With the UPS powered on, you can configure the On‑Battery Indicator Modes by holding down the POWER button and waiting for the third beep. When the third beep sounds, the POWER button will begin cycling red / green. Release the button—its current color indicates the active mode.

Press the POWER button again to cycle through the available modes. Refer to the table below for the three mode‑selection colors. After choosing the desired mode, wait 5 seconds for the UPS to save the setting.

Image showing the power button of the discussed Back UPS ES M Back UPS ES M ON BATTERY Alarm Options

Option 3 : Disable alarms using PowerChute ™ Serial Shutdown for some selected models

You can also configure the UPS audible alarms using PowerChute™ Serial Shutdown (PCSS). Note that PCSS is compatible with the newer Back‑UPS™ models equipped with USB data ports. Also, please note that models with part numbers beginning with BVN typically do not include a USB port.

Additionally, Back‑UPS units will generally work with PCSS when using a Windows operating system (see FAQ000274073 for details). Always check the Compatible Software section on the UPS product page to confirm that your specific model supports PCSS.

An image showing the Back UPS ES M USB port location An image showing the compatible software section that can be possibly found in a Back UPS ES M product page

Location in PowerChute where you can mute a UPS

IMPORTANT NOTE :

A UPS may emit beeping sounds for several possible reasons. Please refer to FA158827.

If you are unsure of the cause or if you are having issues performing the options given above, we recommend contacting our support team for further assistance at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings