How can we help you today?

Default IP Address for SAGE RTU Secure Version (C3414 CPU)

Issue

Users need to know the default factory IP address for a SAGE RTU Secure version after installation or when accessing the device for initial configuration.

Product

SAGE RTU – Secure Version C3414 CPU

Environment

Secure SAGE RTU units in factory‑default state, prior to customer network configuration.
Used in utility, substation automation, and SCADA environments.

Cause

The Secure version of the SAGE RTU ships with a predefined network configuration.
If the end user is unaware of the default IP address, they may be unable to access the web interface or configuration tools for the initial setup.

Resolution

The default IP address from the factory for a SAGE RTU Secure version is:

➡ 192.168.1.1

Users should ensure their PC is configured within the same subnet (e.g., 192.168.1.x) to establish the initial connection.