How can we help you today?

Does updating the ATV930 firmware impact the M580 DDTs or DFBs?

Issue:

Is there any impact on the M580 DDTs or DFBs when updating the ATV930 firmware?

Product Line:

ATV930, ATV630

Environment:

EcoStruxure Control Expert

Resolution:

Updating the ATV930 firmware does not impact the M580 DDTs or DFBs, since these are PLC-side objects

DDTs reference communication mappings, not internal drive memory.

The DDTs in the M580 are built around:

Defined communication objects (control word, status word, references, feedbacks)
Fixed Modbus/TCP or Ethernet/IP register mappings provided by Schneider

They are not tied to the drive’s internal firmware memory layout. Even if the firmware changes internally, the external communication map remains stable.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors