How can we help you today?

How do I troubleshoot a VFD/soft start when the VW3A1111 keypad displays codes instead of full text or say "these files are corrupted"?

When a VFD has a VW3A1111 graphic keypad connected, it only shows codes on the display, such as: QUI, HOM, DAC, LMD, MPA, and so on.

You will need the following for these steps: a computer/laptop and a mini-USB to USB cable.

Instructions:

1. Locate the mini-USB port on the bottom right side of the VW3A1111 keypad and plug in the cable.

2. Connect the cable using a mini USB to USB cable to an available USB port on the PC. The PC should recognize the keypad as an external storage device.

3. Format the keypad.

VW3A1111 format

4. Download the Language files from this link:

http://www.schneider-electric.com/en/download/document/Languages_Drives_VW3A1111/Country Selector | Schneider Electric Global

5. Copy and paste the folders KPCONF and LANG from the package into the Keypad.

Keep in mind that sometimes the LANG folder takes up more memory than what is available on the keypad. If you get an insufficient storage space error when copying the files, please delete some of the language packages located in the LANG folder.

Please be sure the "Fonts.ums" and "en_labels" are copied for English.

VW3A1111 LANG

6. Connect the keypad to the VFD again.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us atdrive.products.support@se.comto create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: