How can we help you today?

How to Install Vijeo Designer v6.2 Base Version and Update it to Service Pack 12.

Issue:

How to Install Vijeo Designer v6.2 Base Version and Update it to Service Pack 12.

Product Line:

Vijeo Designer 6.2

Resolution:

Here’s a download link for Vijeo Designer v6.2 Base Version.

https://www.se.com/us/en/download/document/Vijeo-Designer-V6.2-base/

The Readme file will provide further instructions on how to get the .iso file. You will need 7-Zip to extract the .iso. Once you have the .iso file, you want to right-click and "Mount" it. It will assign it to a temporary letter drive. Then navigate inside the "VJD Installer" folder and run "setup.exe" as admin, or it will not run properly.

During the installation, Vijeo Designer will ask for a reference and serial number. Please put in the following information:

Serial number: 01234567890

Reference number: VJDSNDTGSV62M

This will put the software into a 21 day trial period.

After Vijeo Designer v6.2 is installed, install Service Pack 12 for Vijeo Designer. Make sure you run it as admin. Here is the link:

https://www.se.com/us/en/faqs/FAQ000239885/

(You only need the first attachment. The one that's 384.19MB)

Service Pack 12 will make Vijeo Designer 6.2 free to use, no license needed (SP10 and below do require a license if you need the older versions)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)